You are here: Describing KAS Graphical User Interface > Windows and Panels Overview > Information and Logs

Information and Logs

The Information and Log window is used to identify current state status and can be used to identify operational errors, compilation errors, and also to quickly assist you in finding areas of the workspace or program variables.

This window contains different tabs that provide:

 

Log Messages

Log Messages Settings

Find and Replace

Find and Replace Operations

Browse Variable

Breakpoints

Compiler Output


Stay Connected with Kollmorgen

Copyright © 2015 Kollmorgen™